North America
Enterprise Computing Solutions
lock login
sign up

 

Wyse is the #1 vendor for scalable network-centric computing solutions to the world's largest businesses and institutions. Wyse hardware, software and services ensure customer desktops are secure, reliable and agile, preserving capital and increasing productivity. Wyse elegantly, easily and affordably eliminates these problems at the desktop, which is one of the toughest environments to manage, and as a result, save customers enormous amounts of time and money.


How do we do it?

Wyse builds hardware, software and services that shift computing complexity from the desktop to the network: liberating IT departments from unnecessary support and maintenance functions, empowering users to be more productive and protecting and improving access to critical information and business applications.

Wyse thin clients run Windows, Java, Linux, UNIX and web-based applications safely on central servers using a thin display protocol. Applications do not traverse the network and are not downloaded into the thin client, eliminating user security and bandwidth issues common with PCs. The increased availability of high-bandwidth network connections enable Wyse solutions to run at near desktop speeds -making it easier and more acceptable for business professionals to use Thin Clients in mission-critical applications.

Get the right tool for the right task. Consider the operating systems best for you (Wyse Thin OS, Wyse-enhanced Windows CE, Wyse Linux, Windows XPe) and then the platform (Streamline, Basic, Standard, Expandable, Integrated).

 


Powerful Thin Clients

Adaptable Thin Clients

 

 

Simple thin clients

The Wyse Thin OS is one of the most secure operating systems on the market and is the ideal solution for Citrix ICA (XenApp, Desktop Server and Access Essentials), Microsoft RDP (Terminal Services) and VMware VDI environments. Products included in this family are: V10L and S10.

Wyse S10

The most optimized solution for Citrix ICA (MetaFrame XenApp) and Microsoft RDP (Terminal Services) environments.

It combines great performance, stateless operation, low power consumption, USB ports, remote management, and simple device setup and imaging. This small, lightweight, solid-state (all electronic, with no disk or fan) unit can be mounted out of the way, even on the back of a display, making the S10 ideal for any space-constrained environment.


Wyse V10L

Speed. Performance. Simplicity.

WYSE V series performance is greater than other thin clients

The Wyse V10L's unprecedented speed is this new product's unique differentiator. By combining a fast processor with the ultra-fast, completely secure Wyse Thin OS operating system, boot time is less than 5 seconds and support for Microsoft® Terminal Server, Citrix® Application Delivery and VMware® Virtual Desktop Infrastructure (VDI) architectures is built right in. The Wyse V10L has dual video capability and video performance is fast and crisp. Since no local storage is required, the Wyse V10L is simple to deploy because there is nothing to configure on the desktop, allowing thousands of units to be centrally managed by the already included Wyse Device Manager. With its sleek, space saving design, the Wyse V10L is the perfect desktop solution for data-intensive environments such as those used in the document management, financial services, medical care and research industries.

Products Top

 

Powerful thin clients

Powerful thin clients offer excellent versatility at a great price by delivering server-based computing via Windows CE & Windows CE.NET with a built-in Internet Explorer browser for access to web-based applications. Products included in this family are: S30, V30L & V30LE.

Wyse S30

Innovative, Streamlined Windows CE Thin Client

The Wyse S30 is based on the new Windows CE 5.0 operating system and features a compact, sleek design with high-speed I/O, and innovative attachment system. Products included in this family are: V30L, V30LE.

 

Products Top

Wyse V30L*

Windows CE Performance Delivery with Dual Video Capabilities

The mid-range Wyse V30L combines all of the cost-effective, security rich features that are included in all Wyse Thin Clients with the added benefit of dual video capabilities. The Wyse V30L is powered by Microsoft Windows CE operating system and delivers all of the performance your financial, training or visually intensive application customers need. With its slender design, the Wyse V30L conserves space while enabling users to work across two monitors simultaneously.

 

Products Top

 

Wyse V30LE

Where expandability meets performance and space

The high-range Wyse V30LE thin client delivers the Windows CE performance you need; dual-video support (with purchase of optional monitor splitter cable); 128MB Flash, 128MB DDR2 RAM; a CardBus/PCMCIA slot; plus serial, parallel, and USB ports. Using the same form-factor as the Wyse V class of thin computers, the Wyse V30LE thin client can fit easily into most work environments.

* Monitors not included

Products Top

Adaptable thin clients

An Adaptable thin client that is scalable from a simple appliance to robust workhorse. Products included in this family are: S50, V50L & V50LE

Wyse S50

The World's Most Compact Full Featured Linux-based Thin Client

The Wyse S50 is the smallest, most advanced Linux-based thin client on the market. Complete with the latest Wyse Linux V6 operating system based on Linux Kernel 2.6, the Wyse S50 features a compact, sleek design and feature-rich innovation that is customizable to fit demanding customer needs.

 

Products Top

Wyse V50L*

The Free Roaming Linux Operating System Solution

If Linux V6 is your customer's operating environment, then the Wyse V50L is the suitable choice. With its fast performing CPU, high resolution video, PC/SC smart card reader support and free seating capabilities, the Wyse V50L is the ideal thin client for hospitals, universities, hotels or any business that require users to roam freely and gain secure, instant access to personal desktops from anywhere in the network.

 

Products Top

Wyse V90LE

Where expandability meets performance and space

The high-range Wyse V90LE thin client delivers the Windows XPe performance you need; dual-video support (with purchase of optional monitor splitter cable); a CardBus/PCMCIA slot; plus serial, parallel, and USB ports. Using the same form-factor as the Wyse V90L thin client, the Wyse V90LE thin client can fit easily into most work environments.

 

Products Top


Wyse G90

Thin Client Optimized for Local Applications

Introducing the industry's most powerful thin client. Fast enough to handle the most complex tasks, yet as easy to manage and maintain as any Wyse thin client. You can expand the Wyse G90 thin client with peripherals. The Wyse G90 thin client comes with dual-monitor support standard, and with the option to add more monitors to meet your needs.

 

Products Top


Wyse X90

Extend the benefits of thin computing to mobile users with secure access to corporate networks and IT infrastructure

The Wyse X90 is the advanced mobile thin computer. With a high-performance energy conserving Via C7M ULV processor, the Wyse X90 mobile thin computer gives you all the power and flexibility you need as a mobile user. It comes with a fanless design and no hard disk which means that there are no moving parts and longer lifespan. Other features include a 12.1" Widescreen WXGA TFT LCD screen which delivers the best performance for graphics applications. Because the Wyse X90 mobile thin computer is designed for access to applications that are fully managed in the data center, it is inherently secure from viruses and other malicious software attacks. With a slim design and less than 4lbs of weight it is ideal for the road warriors.

The Wyse X90 mobile thin computer comes with Microsoft® Windows® XP Embedded, giving you access to the most advanced web browser and media player capabilities in a thin computer.

 

Products Top

Wyse X90e

Extend the benefits of thin computing to mobile users with secure access to corporate networks and IT infrastructure

The Wyse X90 is the advanced mobile thin computer. With a high-performance energy conserving Via C7M ULV processor, the Wyse X90 mobile thin computer gives you all the power and flexibility you need as a mobile user. It comes with a fanless design and no hard disk which means that there are no moving parts and longer lifespan. Other features include a 12.1" Widescreen WXGA TFT LCD screen which delivers the best performance for graphics applications. Because the Wyse X90 mobile thin computer is designed for access to applications that are fully managed in the data center, it is inherently secure from viruses and other malicious software attacks. With a slim design and less than 4lbs of weight it is ideal for the road warriors.

The Wyse X90 mobile thin computer comes with Microsoft® Windows® XP Embedded, giving you access to the most advanced web browser and media player capabilities in a thin computer.

In addition, the Wyse X90e mobile thin computer includes Smart Card for security and Bluetooth for internet access through a variety of mobile phone options. Ideal as a desktop thin client replacement for users who need to roam a campus and need access to data to present or collaborate in meetings.

 

Products Top


Wyse X90L

Extend the benefits of thin computing to mobile users with secure access to corporate networks and IT infrastructure

The Wyse X90L augments the portfolio of mobile thin computers that fit customer needs. With a high-performance energy conserving VIA C7-M ULV processor, the Wyse X90L mobile thin computer gives you all the power and flexibility you need as a mobile user. It is the first thin computer with a Gigabit network connectivity for access to the fastest LAN connection possible within your corporate environment. This is a mobile computer designed from the ground-up to meet the thin client criteria, fanless design, no hard disk, no moving parts and longer lifespan.

Other features include a 15.4" Widescreen WXGA TFT LCD screen which provides the real estate needed for normal applications as well as enhanced experience for graphics applications. It provides the flexibility of digital or analog outputs for connecting to the latest projectors or external displays.

Because the Wyse X90L mobile thin computer is designed for access to applications that are fully managed in the data center, it is inherently secure from viruses and other malicious software attacks. With a slim design and less than 5lbs of weight it is ideal for the road warriors. Because the Wyse X90L is more secure, more reliable, and more manageable than a standard laptop or PC, it can provide significant improvements in cost savings and security to any IT implementation. Both mobile thin clients are also 3G capable, allowing access to corporate networks for the road warriors.

The Wyse X90L mobile thin computer comes with Microsoft® Windows® XP Embedded, giving you access to the most advanced web browser and media player capabilities in a thin computer.

This mobile thin computer supports the optional Wyse TCX* software for a superior user experience, including rich multimedia from Windows Terminal Services, Citrix, and VMware VDI architectures.

 

Products Top


Wyse X90Le

Extend the benefits of thin computing to mobile users with secure access to corporate networks and IT infrastructure

The Wyse X90Le augments the portfolio of mobile thin computers that fit customer needs. With a high-performance energy conserving VIA C7-M ULV processor, the Wyse X90Le mobile thin computer gives you all the power and flexibility you need as a mobile user. It is the first thin computer with a Gigabit network connectivity for access to the fastest LAN connection possible within your corporate environment. This is a mobile computer designed from the ground-up to meet the thin client criteria, fanless design, no hard disk, no moving parts and longer lifespan.

Other features include a 15.4" Widescreen WXGA TFT LCD screen which provides the real estate needed for normal applications as well as enhanced experience for graphics applications. It provides the flexibility of digital or analog outputs for connecting to the latest projectors or external displays.

Because the Wyse X90Le mobile thin computer is designed for access to applications that are fully managed in the data center, it is inherently secure from viruses and other malicious software attacks. With a slim design and less than 5lbs of weight it is ideal for the road warriors. Because the Wyse X90Le is more secure, more reliable, and more manageable than a standard laptop or PC, it can provide significant improvements in cost savings and security to any IT implementation. Both mobile thin clients are also 3G capable, allowing access to corporate networks for the road warriors.

The Wyse X90Le mobile thin computer comes with Microsoft® Windows® XP Embedded, giving you access to the most advanced web browser and media player capabilities in a thin computer.

In addition, the Wyse X90Le mobile thin computer includes Smart Card for security and Bluetooth for internet access through a variety of mobile phone options.

This mobile thin computer supports the optional Wyse TCX* software for a superior user experience, including rich multimedia from Windows Terminal Services, Citrix, and VMware VDI architectures.

* Monitors not included

 

Products Top

e software maximizes the security, manageability, affordability, and reliability of your server-centric environment. Products included in this family are Wyse Thin OS, Wyse Device Manager (formerly Rapport), Wyse Streaming Manager & Wyse TCX.

Wyse Thin OS

Wyse Thin OS is ideal for departments and organizations that need support for Citrix ICA, Microsoft RDP, VMware VDI, or Wyse Enterprise Desktop Virtualization environments. It delivers a fast boot time, virus and malware immunity, and outstanding performance in a thin-computing environment.

Wyse Thin OS offers the utmost security and protection from viruses and malicious software because the operating system does not have a publicly exposed API that can be exploited by hackers. Also, since Wyse Thin OS centrally stores and manages all data and applications, desktop devices store no data, further protecting sensitive information. Image management is automated via DHCP and FTP, while Wyse Device Manager (formerly Rapport) handles additional remote device management. For more information download the Wyse Thin OS datasheet.

 

Products Top


Wyse Device Manager

Wyse™ Device Manager device management software, standard with every Winterm thin client, centrally controls a world of intelligent devices - local and remote, wired and mobile, desktop and handheld. It simplifies IT management, reduces TCO, and improves ROI. It is a single software platform that manages a full range of devices - from desktop and tablet thin clients to Palm™ and Pocket PC handheld devices, including PDAs, scanners and other mobile devices. For more information download the Device Manager datasheet.

 

Products Top


Wyse Streaming Manager

Wyse™ Streaming Manager uses streaming technology to deliver software on demand to stateless computing devices. It delivers the power and flexibility of a PC to the user, while giving IT the manageability they want from a thin-computing infrastructure.

Wyse Streaming Manager allows customers to standardize operating system images across their organization and deliver applications based on user roles and responsibilities. Administrators can easily provision new applications or updates to existing applications without having to modify the operating system image, giving them granular control to ensure consistency of deployed software across the enterprise. Download the Streaming Manager datasheet for all the benefits.

 

Products Top


Wyse TCX Suite

Wyse's vision is to provide customers with thin computing benefits without any compromises on the end user experience. Wyse TCX is the cornerstone to delivering on this vision. It provides an "Enrichment" component within the thin computing infrastructure during the access to corporate applications -- irrespective of the backend infrastructure used to access them.

There are a number of different components in this overall brand of solutions that are being developed by Wyse. All Wyse TCX solutions are agnostic of the backend infrastructure so customers can get access to this solution when they are connecting to any of the following datacenter solutions prevalent in the market: Microsoft Terminal Services, Citrix Presentation Server and VMware Virtual Desktop Infrastructure.

The following components are now available:

Wyse TCX Multimedia

Wyse TCX Multimedia 2.0 software provides rich multimedia playback capabilities within an ICA or RDP environment. TCX Multimedia is a software layer on the server that intelligently redirects the multimedia processing tasks dynamically between the client and server. The multimedia stream decodes locally on the client using the local processing power of the device thereby providing complete multimedia playback capabilities overcoming any limitations that are inherent in traditional thin computing architectures. The Wyse TCX multimedia reduces the server load as well as the network bandwidth as the streams can be directly delivered to the client from a local media server rather than through the datacenter. For more information download the Wyse TCX Multimedia datasheet.


Wyse TCX Multi-display

Wyse TCX Multi-display 1.1 streamlines the user experience of an end-user while working across multiple screens within a ICA/RDP connection. Wyse TCX multi-display software is deployed on the server side and a client side component is deployed in the local operating system on the client side.

The solution works in the "span" mode i.e. a RDP/ICA desktop connection that is extended so that the same desktop is spread across 4 monitors. Wyse TCX Multi-display software provides the windowing capabilities that makes the desktop multiple monitor aware. In version 1.1, the TCX Multi-display software is made and restricted to Wyse device use only. The software makes sure that the maximization of a window within the desktop is limited to only 1 screen (rather than across both screens without Wyse TCX software) and the dialog boxes/popup windows are also centered on the appropriate window. Wyse TCX software provides the same user experience as that of a local XP Pro session on a PC with 2 or 4 monitors enabled. For more information download the Wyse TCX Multi-display datasheet.


Wyse TCX USB Virtualizer

Wyse TCX USB Virtualizer 1.0 is a revolutionary software solution that enables the sharing and discovery of local USB devices plugged into Wyse thin clients as if they were connected directly on the Virtualized Desktop environment. The extraordinary enhancement solves the USB peripheral issues when it comes to deploying thin clients. No more compromise on limited local drivers. The Wyse thin clients now can seamlessly access their USB-based printers, scanners, storage devices, Palm, BlackBerry, and Pocket PC hand­helds over VDI environment The enhancement is available for Wyse Thin OS and XP Embedded platforms. For more information download the Wyse TCX USB Virtualizer datasheet.

 

Using a virtual desktop server-based infrastructure decreases employee's downtime since all trouble shooting, management and control can be handled efficiently from a central location. A virtual server set up greatly reduces the risk of viruses by allowing your IT experts to build the proper infrastructure in order to create a more secure environment. Wyse EDV also overcomes the hesitation of giving up a personal operating system and applications, since all operating systems, such as Windows XP Professional or Vista, execute independently for each desktop. Since each desktop has its own dedicated virtual machine a user will maintain their personalized desktop and applications while not conflicting with other users.

The key is to take the extra step in a virtual environment. A complete desktop virtual solution features a desktop device that can leverage this architecture, while maintaining the security and management levels you put in place.

How It Works

  1. Start with the Server
    The first thing you need is a virtual desktop server and desktop virtualization solution. The Wyse EDV solution works at the desktop, offering a simple solution that dramatically improves IT staff productivity. Desktop virtualization puts a thin layer of software is between the server hardware and the operating system. This supports the management of multiple virtual machines within the server: each virtual machine with its own operating system and applications. The Wyse EDV solution then assigns each thin computer its own virtual machine on the server.
  2. Address the desktop
    At the desktop, the Wyse thin computer works just like a standard PC. The Wyse S10-VDI Edition is connection-broker aware, so it automatically finds its virtual desktop on the server. Your Wyse thin computers are also centrally managed and accessible from anywhere on the network. The Wyse Thin OS-VDI Edition also delivers the utmost security and protection from viruses and malicious software because the software does not have a publicly exposed API that can be exploited by hackers.
  3. The Wyse 25-Seat Pilot in a Box will allow you to take the first step to tackle the challenges you face on a daily basis at the desktop. All you need are the minimum hardware and software specifications for your virtual environment, the pilot in a box, and two days to work with a system engineer to get started. This solution will allow you to see immediate results and drive you to build the needed business case to move forward with a full deployment of Wyse Enterprise Virtualized Desktop environment. Click for more information on Pilot in a Box.
 

Products Top


None at this time

Quicklinks



There are no specials at this time